Hi
I used S32K312 and there is a problem to select I2C Clock Source
Even though i set the clock source to 30Mhz and active, i2c clcok source candidates are not identified when i set i2c peripheral.
candidate group of SPI could selected without any problems, can you help me?
MCU : S32K312NHT0MPASR
IDE : Design Studio 3.6.2
RTD : S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 6.0.0 (Latest by current standards)
Solved! Go to Solution.
Hi
It looks similar to the previous question, please refer to the screenshot in that question: s32k312 I2C Clock Source
Please add Clock_Ip_ReferencePoints in Peripherals tool and configure AIPS_SLOW_CLK as the MODULE_CLK source of LPI2C.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi
It looks similar to the previous question, please refer to the screenshot in that question: s32k312 I2C Clock Source
Please add Clock_Ip_ReferencePoints in Peripherals tool and configure AIPS_SLOW_CLK as the MODULE_CLK source of LPI2C.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------