Hi There.
I need to split the only Block0 (512kB) present in s32k310 in two parts: bootloader and application part.
Running bootloader, I need to erase/program application sectors and I need to load Erase and program functions to ".ramcode " (then .itcm later because SRAM is so small... ) because of a unique block0 available.
I have a lot of problem by placing RTDs functions in "ramcode, "
Using an" attibute_section" near each function is ok but it makes the code unmaintainable when newer RTDs are available.
A much affordable approach is to replace MEM_43_INFLS_START_SEC_CODE/MEM_43_INFLS_END_SEC_CODE with MEM_43_INFLS_START_SEC_RAMCODE/MEM_43_INFLS_END_SEC_RAMCODE in C40_ip.c
and
RTE_START_SEC_CODE/ RTE_STOP_SEC_CODE with RTE_START_SEC_RAMCODE/ RTE_STOP_SEC_RAMCODE in SchM_Mem_43_INFLS.c (called by C40_Ip)
but, tacking a look to map file, not all the funcions included (in those sections SRART/STOP) are placed in ".ramcode" section. and are still placed in .mcal_text.
In particular no one of the the functions I need is placed in ramcode.
Is it available a method useful to place s32k310 RTDs in ram ? Maybe I miss something.... Otherwise it is not possible to erase sectors of the same block in s32l310 (a bus fault hard exception always occours ) in an mantainable manner.
Best regards
Fabio
已解决! 转到解答。
Hi @FabioG,
Yes, unfortunately this fix is needed for each RTD release as the default location is flash, but if you are not in need of the minor updates, you can keep working with the full RTM release of the RTD (5.0.0, for example) and keep the changes you've made.
Best regards,
Julián
Hi @FabioG,
The methods you mentioned are the recommended ways to place functions in ram, please see these two community posts:
Could you please follow the steps in those community posts and confirm again if the functions are correctly displayed in the map file?
Best regards,
Julián
Hi @FabioG,
Yes, unfortunately this fix is needed for each RTD release as the default location is flash, but if you are not in need of the minor updates, you can keep working with the full RTM release of the RTD (5.0.0, for example) and keep the changes you've made.
Best regards,
Julián