s32k3 advanced boot temporarily stopped when OTA?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k3 advanced boot temporarily stopped when OTA?

Jump to solution
597 Views
victory
Contributor IV

Hi NXP

   as title, if one SMR is linked to a app region and enabled periodic check,  how to handle this case, is there any sample for reference? thanks.

0 Kudos
Reply
1 Solution
509 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

This HSE service can be used:

lukaszadrapa_0-1732531409659.png

 lukaszadrapa_1-1732531418006.png

But I can't see API for this function, so it should be implemented by user if needed.

Regards,

Lukas

 

View solution in original post

0 Kudos
Reply
3 Replies
553 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @victory 

There's not an option to stop periodic check. It would be necessary to erase such SMR and then install it again.

And because there's sentence in the API RM:

"If the periodic SMR verifi cation is used, the HSE fi rmware always uses the internal hash for verification."

... that means that you can't use AuthTag placed on constant address during AB swap, so it will be necessary to reinstall the SMR anyway.

Regards,

Lukas

0 Kudos
Reply
535 Views
victory
Contributor IV

thanks for your reply, and what's the api of "erase such SMR "?

0 Kudos
Reply
510 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

This HSE service can be used:

lukaszadrapa_0-1732531409659.png

 lukaszadrapa_1-1732531418006.png

But I can't see API for this function, so it should be implemented by user if needed.

Regards,

Lukas

 

0 Kudos
Reply