s32k144 port interrupt wakeup form vlps

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k144 port interrupt wakeup form vlps

2,167 Views
1090097669
Contributor III

Hello every one:

 

 Recently,I have some problems on RUN and VLSP mode configuration, I am the following information is correct:
1. S32K144 chips do not have CAN RXD wake function module

2. Before enter VLSP mode, need to configure the RTC CLOCK module

and The following is my adopted the SDK software configuration module:

static void gpio_port_int_init(void)
{
INT_SYS_EnableIRQ(PORTB_IRQn);
INT_SYS_InstallHandler(PORTB_IRQn, &gpio_portb_irq, (isr_t *)0);

INT_SYS_EnableIRQ(PORTD_IRQn);
INT_SYS_InstallHandler(PORTD_IRQn, &gpio_portd_irq, (isr_t *)0);

INT_SYS_EnableIRQ(PORTE_IRQn);
INT_SYS_InstallHandler(PORTE_IRQn, &gpio_porte_irq, (isr_t *)0);

PINS_DRV_SetPinIntSel(GPIO_CP_UNLOCK_PORT,GPIO_CP_UNLOCK_PIN,PORT_DMA_INT_DISABLED);
PINS_DRV_SetPinIntSel(GPIO_CP_WAKE_PORT,GPIO_CP_WAKE_PIN,PORT_DMA_INT_DISABLED);
PINS_DRV_SetPinIntSel(GPIO_CC_WAKE_PORT,GPIO_CC_WAKE_PIN,PORT_DMA_INT_DISABLED);
PINS_DRV_SetPinIntSel(GPIO_VCU_WAKE_PORT,GPIO_VCU_WAKE_PIN,PORT_DMA_INT_DISABLED);
}

void init_NVIC(void)
{

PINS_DRV_SetPinIntSel(PORTE,5U,PORT_INT_RISING_EDGE);

}

void Power_RUN_to_STOP (void)
{

PMC->REGSC |= PMC_REGSC_BIASEN(1); // [1] CLKBIASDIS = 1 In VLPS mode, the bias current for SIRC, FIRC, PLL is disabled
/* Disable the Fosc and Sosc from chip*/
SCG->FIRCCSR = SCG_FIRCCSR_FIRCEN(0);
while(SCG->FIRCCSR & (1 << 24));
SCG->SOSCCSR = SCG_SOSCCSR_SOSCEN(0);

S32_SCB->SCR |= S32_SCB_SCR_SLEEPDEEP_MASK|0x2; /* allow deep sleep mode0 */
SMC->PMPROT = SMC_PMPROT_AVLP(1); /* allow very low power mode*/


SMC->PMCTRL = SMC_PMCTRL_STOPM(2);

if(SMC->PMSTAT == 0x01)
{
asm("WFI");
}


}

 

void power_set_mode(POWER_SYS_TYPE mod)
{
if(mod == POWER_SYS_SLEEP)
{

init_NVIC();
//power_can_wakeup_set();
POWER_SYS_SetMode(POWER_SYS_VLPS, POWER_MANAGER_POLICY_AGREEMENT);
}
}

 

Regards,

Katrinal

Tags (4)
1 Reply

1,474 Views
nyf
Contributor I

不好意思,麻烦问一下,我这边使用142也出现了同样的问题,在设置完低功耗模式之后,电流仍然降不下来,麻烦问一下,您具体是怎么解决这个问题的

0 Kudos
Reply