Any sample code is available for low voltage detection interrupt for S32K144.
How to configure LVD interrupt in CT.
Used RTD version: SW32K1_RTD_4_4_1_0_1_D2202
Hello @SivaB,
I'm sorry for the delay.
Please find a test project attached.
I have found and reported a few issues both in RTD 1.0.1 and 2.0.0 while testing it.
The driver does not clear the flags correctly:
Regardless of LVD or LVW, the driver return the same error code:
The Power_Ip driver does not clear LVDF after POR before LVD interrupt is enabled.
Regards,
Daniel
Any sample code is available for low voltage detection interrupt for S32K144.
How to configure LVD interrupt in CT.
Used SDK version: SW32K1_S32DS_3.4.1_D2106