Chipset: S32K144HAT0VLH
Function: FLEXCAN
TXD (PTC3)
RXD (PTC2)
Implementation:
Implementation of communication without using CAN transceiver.
Question:
Is there a method or manual to check the impedance of TXD and RXD pins?
Thanks.
解決済! 解決策の投稿を見る。
Hi,
TXD (PTC3) / RXD (PTC2) are normal IO pins so refer to datasheet for I/O parameters.
If you want to connect nodes without transceiver on short distance on PCB below connection is commonly used
BR, Petr
Hi,
TXD (PTC3) / RXD (PTC2) are normal IO pins so refer to datasheet for I/O parameters.
If you want to connect nodes without transceiver on short distance on PCB below connection is commonly used
BR, Petr