s32k144的can0使能can fd后,can1和can2就不能用了吗?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k144的can0使能can fd后,can1和can2就不能用了吗?

Jump to solution
975 Views
fedora
Contributor III

您好:

  我的环境是s32 ds,使用PE配置外设,代码中3个can都初始化了,但如果在PE中使能can0的fd,烧写固件后不能运行,不使能can0 fd就可以运行; 另外,如果使能can0的fd,但不初始化can1和can2,固件也是可以运行的;

   我想确认的问题是:如果使能can0的fd,那么can1和can2就不能使用了吗?

谢谢!

0 Kudos
Reply
1 Solution
954 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@fedora

没有这样的限制,这还是你什么地方配置的不对

View solution in original post

0 Kudos
Reply
2 Replies
955 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@fedora

没有这样的限制,这还是你什么地方配置的不对

0 Kudos
Reply
949 Views
fedora
Contributor III

好的,感谢确认,我再找找原因!

0 Kudos
Reply