s32k118 dynamically changing the frequency of pwm output.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32k118 dynamically changing the frequency of pwm output.

932件の閲覧回数
SteveSam
Contributor II

hi,

i want to change the frequency of the pwm output in the code from 1000 to 2000 and back to 1000. in the examples i can see dutycycle being changed . but i could not find frequency being changed. please help me....

Regards,

Steve

 

0 件の賞賛
返信
1 返信

900件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Steve,

Please refer to the discussion in Changing FTM_PWM period and duty cycle


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信