1. Thank you for your feedback. I re-request the relevant department to attach the schematic of the S32K116EVB2Q048
2. I did not find the BOM of S32K116EVB2Q048, but you may refer to the BOM of S32K116EVB-Q048 S32K116EVB-QSP
Thank you @Robin_Shen
Can you correct the schematic for the same in the Get Started with the S32K116EVB2Q048 | NXP Semiconductors.
Currently I see the schematic for S32K144EVB as seen below -
Hi @Robin_Shen
1. Looks like the schematic has been updated to S32K116. But it looks like the schematic is for different version. EVB vs EVB2. Please verify for the same.
2. Is it possible to get the BOM for the EVB board ?
1. Thank you for your feedback. I re-request the relevant department to attach the schematic of the S32K116EVB2Q048
2. I did not find the BOM of S32K116EVB2Q048, but you may refer to the BOM of S32K116EVB-Q048 S32K116EVB-QSP
Hi
For S32K116EVB2Q048, SCH-47484.pdf is correct schematic. The latest S32K1xx SDK select PTA7 (ADC0_SE3) sample the Potentiometer. But the R750 is DNP, you need to solder it by your self..
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------