s32k116 evb adc pot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k116 evb adc pot

Jump to solution
2,468 Views
yjp312
Contributor I

I am using #S32K116 Eval Board - S32K116EVB2Q048. 

The board has one ADC_POT, but it looks there is no connection. Can you help me if I am looking at the correct schematic. And if so, how to observe the change in POT values when programming on S32K. 

0 Kudos
1 Solution
2,324 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

1. Thank you for your feedback. I re-request the relevant department to attach the schematic of the S32K116EVB2Q048

2. I did not find the BOM of S32K116EVB2Q048, but you may refer to the BOM of S32K116EVB-Q048 S32K116EVB-QSP

View solution in original post

0 Kudos
5 Replies
2,455 Views
yjp312
Contributor I

Thank you @Robin_Shen 

Can you correct the schematic for the same in the Get Started with the S32K116EVB2Q048 | NXP Semiconductors. 

Currently I see the schematic for S32K144EVB as seen below - 

yjp312_0-1661505244775.png

 




0 Kudos
2,332 Views
yjp312
Contributor I

Hi @Robin_Shen 

1. Looks like the schematic has been updated to S32K116. But it looks like the schematic is for different version. EVB vs EVB2. Please verify for the same.

2. Is it possible to get the BOM for the EVB board ?

0 Kudos
2,325 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

1. Thank you for your feedback. I re-request the relevant department to attach the schematic of the S32K116EVB2Q048

2. I did not find the BOM of S32K116EVB2Q048, but you may refer to the BOM of S32K116EVB-Q048 S32K116EVB-QSP

0 Kudos
2,439 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Thank you for the report, I'll inform related team about this.

0 Kudos
2,464 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

For S32K116EVB2Q048, SCH-47484.pdf is correct schematic. The latest S32K1xx SDK select PTA7 (ADC0_SE3) sample the Potentiometer. But the R750 is DNP, you need to solder it by your self..

Get Started with the S32K116EVB2Q048.png

R750 ADC_POT S32K116EVB2Q048.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------