s32k116 can not use all ram

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32k116 can not use all ram

801件の閲覧回数
Harold_zhou
Contributor II

364713ca-ed28-4d46-9d1f-da82ceb8f2a1.png I set the configTOTAL_HEAP_SIZE = 4096 in freertosConfig.h ,the project can build successfully.if I set the configTOTAL_HEAP_SIZE = 8192,the project show error:S32k116_Freertos.elf section `.bss' will not fit in region `m_data_2'

region m_data_2 overflowed with stack and heap

section .stack VMA [20003600,200037ff] overlaps section .bss VMA [200020c0,200042a3]

region `m_data_2' overflowed by 0 bytes

when it is 8192 ,the ram used only almost 9 KB, less than the total ram space 16kB.why does it remind error,how to solve it?

0 件の賞賛
返信
3 返答(返信)

781件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Harold_zhou,

Do you really use the RAM linker file that you posted or is it the Flash linker file?

Anyway, there is only 0x37FF of SRAM_U.

The heap is in m_data_2 memory area. So, if you need 8kB heap, you need at least 8kB (0x1FFF) of m_data_2. 

But there is BSS and the stack in m_data_2 too.

 

Regards,

Daniel

 

 
 

 

 

 

 

0 件の賞賛
返信

766件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Harold_zhou,

 

The error message mentioned m_data_2 which is in the *flash.ld linker file only.

So, you use the *flash.ld linker in the project not the *ram.ld

You can increase m_data_2 but only within the size of the actual SRAM_U as I mentioned.

 

Regards,

Daniel

 

0 件の賞賛
返信

773件の閲覧回数
Harold_zhou
Contributor II

it is ram link file,so I need change the m_data_2 in linker file named flash.ld 

 

/* SRAM_U */
m_data (RW) : ORIGIN = 0x20000000, LENGTH = 0x000020C0
m_data_2 (RW) : ORIGIN = 0x200020C0, LENGTH = 0x00001740

タグ(1)
0 件の賞賛
返信