s32k can1 is not work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k can1 is not work

2,662 Views
xuzeze
Contributor I

S32K can1 not work ,can0 is ok.My mcu is s32k144-64pins . The following is my code :

void FlexCAN_init_IRQs(void) {
//can0
    FSL_NVIC->ICPR[2] = 1 << (CAN0_ORed_0_15_MB_IRQn % 32); /*  ch0: clr any pending IRQ*/
    FSL_NVIC->ISER[2] = 1 << (CAN0_ORed_0_15_MB_IRQn % 32); /*  ch0: enable IRQ */
    FSL_NVIC->IP[CAN0_ORed_0_15_MB_IRQn] = 0xA;             /*  ch0: priority 10 of 0-15*/
//can1
    FSL_NVIC->ICPR[2] = 1 << (CAN1_ORed_0_15_MB_IRQn % 32); /*  ch0: clr any pending IRQ*/
    FSL_NVIC->ISER[2] = 1 << (CAN1_ORed_0_15_MB_IRQn % 32); /*  ch0: enable IRQ */
    FSL_NVIC->IP[CAN1_ORed_0_15_MB_IRQn] = 0xA;             /*  ch0: priority 10 of 0-15*/

}

void CAN1_ORed_0_15_MB_IRQHandler() {
    /* Read message */

    FLEXCAN1_receive_msg();
}

void FlexCAN_PORT_init(void) {

    PCC->PCCn[PCC_PORTC_INDEX] |= PCC_PCCn_CGC_MASK;
    PCC->PCCn[PCC_PORTD_INDEX] |= PCC_PCCn_CGC_MASK;
    PCC->PCCn[PCC_PORTE_INDEX] |= PCC_PCCn_CGC_MASK; /* Enable clock for PORTE */
    //CAN 0
    PORTC->PCR[2] |= PORT_PCR_MUX(3); /*  CAN0_RX */
    PORTC->PCR[3] |= PORT_PCR_MUX(3); /*  CAN0_TX */
    PORTD->PCR[7] |= PORT_PCR_MUX(1); /*  CAN0_STAND*/
    //CAN 1
    PORTC->PCR[6] |= PORT_PCR_MUX(3); /*  CAN1_RX */
    PORTC->PCR[7] |= PORT_PCR_MUX(3); /*  CAN1_TX */
    PORTE->PCR[6] |= PORT_PCR_MUX(1); /*  CAN1_STAND*/
    //can2
    PORTC->PCR[16]|= PORT_PCR_MUX(3); /*  CAN2_RX */
    PORTC->PCR[17]|= PORT_PCR_MUX(3); /*  CAN2_TX */

    PTD->PDDR |= 1 << 7;
    PTE->PDDR |= 1 << 6;
    PTD->PCOR |= 1 << 7;
    PTE->PCOR |= 1 << 6;
//  can mode sel
    CAN0_NORMAL();
    CAN1_NORMAL();
}

void FLEXCAN0_init(uint32_t speed_value) {

    uint32_t i = 0;

    PCC->PCCn[PCC_FlexCAN0_INDEX] |= PCC_PCCn_CGC_MASK; /* CGC=1: enable clock to FlexCAN0 */
    CAN0->MCR |= CAN_MCR_MDIS_MASK; /* MDIS=1: Disable module before selecting clock */
    CAN0->CTRL1 &= ~CAN_CTRL1_CLKSRC_MASK; /* CLKSRC=0: Clock Source = oscillator (8 MHz) */
    CAN0->MCR &= ~CAN_MCR_MDIS_MASK; /* MDIS=0; Enable module config. (Sets FRZ, HALT)*/
    while (!((CAN0->MCR & CAN_MCR_FRZACK_MASK) >> CAN_MCR_FRZACK_SHIFT)) {
    }
    CAN0->CTRL1 = speed_value;
    for (i = 0; i < 64; i++) { /* CAN0: clear 32 msg bufs x 4 words/msg buf = 128 words*/
        CAN0->RAMn[i] = 0; /* Clear msg buf word */
    }
    for (i = 0; i < 16; i++) { /* In FRZ mode, init CAN0 16 msg buf filters */
        /*Configure based on need*/
        CAN0->RXIMR[i] = 0; /* Check all ID bits for incoming messages */
    }
    CAN0->RXMGMASK = 0; /* Global acceptance mask: check all ID bits */
    /*Change the masking based on MLC adress*/
    CAN0->RAMn[4 * MSG_BUF_SIZE + 0] = 0x04000000; /* Msg Buf 4, word 0: Enable for reception */

    CAN0->RAMn[4 * MSG_BUF_SIZE + 1] = 0x14440000; /* Msg Buf 4, word 1: Standard ID = 0x111 */
    CAN0->RAMn[2 * MSG_BUF_SIZE + 0] = 0x04000000; /* Msg Buf 4, word 0: Enable for reception */

    CAN0->RAMn[2 * MSG_BUF_SIZE + 1] = 0x14440000; /* Msg Buf 4, word 1: Standard ID = 0x111 */
    CAN0->RAMn[3 * MSG_BUF_SIZE + 0] = 0x04000000; /* Msg Buf 4, word 0: Enable for reception */
    CAN0->RAMn[3 * MSG_BUF_SIZE + 1] = 0x14440000; /* Msg Buf 4, word 1: Standard ID = 0x111 */

    /* PRIO = 0: CANFD not used */
    CAN0->MCR = 0x0002001F; /* Negate FlexCAN 1 halt state for 32 MBs */
    CAN0->IMASK1 = 0x0000001C;
    while ((CAN0->MCR && CAN_MCR_FRZACK_MASK) >> CAN_MCR_FRZACK_SHIFT) {
    }
    /* Good practice: wait for FRZACK to clear (not in freeze mode) */
    while ((CAN0->MCR && CAN_MCR_NOTRDY_MASK) >> CAN_MCR_NOTRDY_SHIFT) {
    }
    /* Good practice: wait for NOTRDY to clear (module ready)*/
}

void FLEXCAN1_init(uint32_t speed_value) {
    uint32_t i = 0;

    PCC->PCCn[PCC_FlexCAN1_INDEX] |= PCC_PCCn_CGC_MASK; /* CGC=1: enable clock to FlexCAN1 */
    PCC->PCCn[PCC_FlexCAN1_INDEX] = PCC_PCCn_CGC_MASK; /* CGC=1: enable clock to FlexCAN0 */


    CAN1->MCR |= CAN_MCR_MDIS_MASK; /* MDIS=1: Disable module before selecting clock */
    CAN1->CTRL1 &= ~CAN_CTRL1_CLKSRC_MASK; /* CLKSRC=0: Clock Source = oscillator (8 MHz) */
    CAN1->MCR &= ~CAN_MCR_MDIS_MASK; /* MDIS=0; Enable module config. (Sets FRZ, HALT)*/

    while (!((CAN1->MCR & CAN_MCR_FRZACK_MASK) >> CAN_MCR_FRZACK_SHIFT)) {
    }
    CAN1->CTRL1 = speed_value;
    for (i = 0; i < 64; i++) { /* CAN1: clear 16 msg bufs x 4 words/msg buf = 64 words*/
        CAN1->RAMn[i] = 0; /* Clear msg buf word */
    }
    for (i = 0; i < 16; i++) { /* In FRZ mode, init CAN1 16 msg buf filters */
        CAN1->RXIMR[i] = 0; /* Check all ID bits for incoming messages */
    }

    CAN1->MCR = 0x0002000f; /* Negate FlexCAN 1 halt state for 16 MBs */
    CAN1->IMASK1 = 0x0000000f;

    while ((CAN1->MCR && CAN_MCR_FRZACK_MASK) >> CAN_MCR_FRZACK_SHIFT) {
    }
    /* Good practice: wait for FRZACK to clear (not in freeze mode) */
    while ((CAN1->MCR && CAN_MCR_NOTRDY_MASK) >> CAN_MCR_NOTRDY_SHIFT) {
    }
    /* Good practice: wait for NOTRDY to clear (module ready)*/
}

Tags (1)
4 Replies

495 Views
aurrutia
Contributor I

Same issue on EVB S32K144 eval kit. I am trying to work with 2 instances of CAN:

  • CAN 0 for RX FIFO to communicate with Kvaser CAN Analyzer (I am using the connector J13 output of SBC)
  • CAN 1  for TX to an external transceiver (I am using PTA12 and PTA13).

The error is the same, CAN0 works as expected but I can't see anithing with the osciloscope on PTA12 (TX) CAN1. Why could be the reason? I try to Transmit over the CAN0 MB 9 (because the RX FIFO is 8 MBs) and it works well, but in the CAN1 I can't see anything.

I also have checked to send a message over PTA12 and PTA13  together to see if it is properly initialized, the oscilocope show that there is a wavefrom similar to CAN, but when I try to send something and check the pin PTA12 (tx), the osciloscope shows nothing.

0 Kudos
Reply

1,859 Views
songwanjie
Contributor I

 __IO uint32_t RXIMR[CAN_RXIMR_COUNT]; 

CAN_RXIMR_COUNT =32 ;but when CAN_RXIMR_COUNT>16 , it is wrong;

0 Kudos
Reply

1,859 Views
PetrS
NXP TechSupport
NXP TechSupport

yes, it could be. There are just 16 MBs (and so RXIMRs) implemented on the FlexCAN1 module.

FlexCAN0 has 32 MBs.

pastedImage_1.png

BR, Petr

0 Kudos
Reply

1,859 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

Could you please specify in more details what is not working on CAN1? It is used to send or receive frames? There is no MB prepared for RX or TX.

Do you use own board? How is the module connected to the bus?

BR, Petr