Hi,
I have a S32K3X4EVB, and I try to download a example program by its OpenSDA, but the Windows on my laptop doesn't probe this device. When I plugin the micro-USB, the D15 LED (i.e. RST_OSDA) will blink, but there is no OpenSDA device present in my Windows device manager. Should I change any jumper for OpenSDA? the jumpers on the EVB are default setting.
And I tried to debug the S32K344 on the EVM with PE's CycloneFX, it works fine.
I also have a S32K144EVB board, the OpenSDA is work properly on my laptop.
My S32DS version is 3.4.3 with S32K3xx development package 1.0.0.
Thank you,
Snaku
已解决! 转到解答。
Hi,
with respect of drivers on PC, be sure you have S32K3 development package installed
Regarding K26 FW reflashing; it will be better to ask Pemicro support directly for giving latest FW and guide; https://www.pemicro.com/support
BR, Petr
Hi,
default jumper setting is mentioned in board user manual https://www.nxp.com/webapp/Download?colCode=S32K3X4EVB-Q172_HW-UM. Also you can try to follow Getting started guide; https://www.nxp.com/document/guide/getting-started-with-the-s32k3x4evb-q172-evaluation-board:GS-S32K...
After USB cable is connected below should appear in PC device manager
and this is then selected in debug configuration
BR, Petr
Hi Petr,
My Windows doesn't detect the 'Multilink' device when I connect a micro-USB cable, and I check the jumpers setting with the 'getting start' page, they are in default position.
I think maybe the 'OpenSDA' firmware in the K26 MCU is gone, if it was true, how do i reflash the K26 firmware? could you provide the web page?
Thank you,
Snaku
Hi,
with respect of drivers on PC, be sure you have S32K3 development package installed
Regarding K26 FW reflashing; it will be better to ask Pemicro support directly for giving latest FW and guide; https://www.pemicro.com/support
BR, Petr