I use MCAL S32K14X_MCAL4_2_RTM_P4_1_0_1 Tresos:24.0.0
but it shows below err
ERROR 20-08-27,17:07:57 (1803) Invalid XPath-expression for Attribute "READONLY" of node "/AUTOSAR/TOP-LEVEL-PACKAGES/ActiveEcuC/ELEMENTS/Port/PortGeneral/PortSet2PinsDirectionApi": (35016) Cannot get a resource file for target ARM and derivate S32K14X. Maybe this is due to module restrictions. Errors "1" Warnings "21"
Hello,
This issue is fixed in RTM 1.0.2 and above. I suggest you to use the version from 1.0.2 and above, and see whether the issue still occurs.
Best Regards,
Nam