jlink flash programming S32K344

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

jlink flash programming S32K344

747 次查看
monk_65
Contributor III

 

hello,

 

i use the MR-CANHUBK344 development board with a segger jlink, and i have the same problem of this post

https://community.nxp.com/t5/S32K/S32K344-RTD-PORT-DIO-and-Debugging/td-p/1693264

is the jumper JP1 must be remove to program the board ?

i tried

r0

erase

but it don't work

the file .elf is the demo MR_CANHUBK3_IEEE1722

here the message


Connecting to target via C2
ConfigTargetSettings() start
ConfigTargetSettings() end - Took 24us
InitTarget() start
Unknown SDA AP Id detected: 0xFFFFFFFF
InitTarget() end - Took 2.62ms
Connect failed. Resetting via Reset pin and trying again.
ConfigTargetSettings() start
ConfigTargetSettings() end - Took 13us
InitTarget() start
Unknown SDA AP Id detected: 0xFFFFFFFF
InitTarget() end - Took 1.97ms

 

 

 

 

 

 

 

0 项奖励
回复
0 回复数