i want linker file and startup file for S32K118 .

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i want linker file and startup file for S32K118 .

1,671 Views
ibrahim_elaasy
Contributor II

i want linker file and startup file for S32K118 be compatible with MCAL SDK  .

i want to add my object files for certain section on Flash Memory and in RAM manually .

Labels (1)
0 Kudos
2 Replies

633 Views
esser
Contributor I

Hello,

i didn't find the files (linker and startup)in the defined path when i downlaod the MCAL autosar for s32 k from NXP website 

 

0 Kudos

1,439 Views
frantisekdobes
NXP Employee
NXP Employee

The MCAL4.2 and MCAL4.3 releases contain sample application for S32K118 which includes startup and linker files. After you install the MCAL4.2 it is available here:
c:\NXP\AUTOSAR\S32K14X_MCAL4_2_RTM_1_0_1\S32K14X_MCAL4_2_RTM_1_0_1_Sample_Application\eclipse\plugins\IntegrationFramework_TS_T40D2M10I1R0\auxiliary\toolchains
Or if you use MCAL4.3 then it is available here:
c:\NXP\AUTOSAR\S32K14X_MCAL4_3_RTM_1_0_0\S32K14X_MCAL4_3_RTM_1_0_0_Sample_Application\eclipse\plugins\IntegrationFramework_TS_T40D2M10I0R0\auxiliary\toolchains

The MCAL4.0 release contains sample application for S32K144 only.


You could also take the linker and startup files from S32 Design Studio for ARM which is available for free from www.nxp.com. After you install S32DS the linker and startup files are available here (if installed to the default path):
c:\NXP\S32DS_ARM_v2018.R1\S32DS\S32SDK_S32K1xx_RTM_3.0.0\platform\devices\S32K118