how to use the EB Tresos generates the code--(EB Tresos Studio 27.1.0)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to use the EB Tresos generates the code--(EB Tresos Studio 27.1.0)

ソリューションへジャンプ
5,340件の閲覧回数
Guofred
Contributor III

Open EBTresos and click File -> Import -> General -> Existing Projects 
into Workspace
, select the template project McAl_template_project_dio_47811a_440_100. zip installation Path into which the Tresos project is imported.  when i click the somld , some error comes out .the details as below. 

Guofred_3-1639652849687.png

Guofred_4-1639652952145.png

Guofred_5-1639653007689.png

What causes this problem and how can I fix it, thanks.

Best regards.

Guofred

 

 

 

0 件の賞賛
返信
1 解決策
5,322件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

The problem is EB Tresos couldn't find the MCAL package. You need to install the MCAL package which correspond to the project you're using, by copy to the EB/tresos/plugins folder.

Best Regards,

Nam

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
5,323件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

The problem is EB Tresos couldn't find the MCAL package. You need to install the MCAL package which correspond to the project you're using, by copy to the EB/tresos/plugins folder.

Best Regards,

Nam

0 件の賞賛
返信
5,318件の閲覧回数
Guofred
Contributor III

Hi @namnguyenviet ,

Ok, thanks for your help.

Best regards.

Guofred 

0 件の賞賛
返信