how to use the EB Tresos generates the code--(EB Tresos Studio 27.1.0)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to use the EB Tresos generates the code--(EB Tresos Studio 27.1.0)

Jump to solution
5,133 Views
Guofred
Contributor III

Open EBTresos and click File -> Import -> General -> Existing Projects 
into Workspace
, select the template project McAl_template_project_dio_47811a_440_100. zip installation Path into which the Tresos project is imported.  when i click the somld , some error comes out .the details as below. 

Guofred_3-1639652849687.png

Guofred_4-1639652952145.png

Guofred_5-1639653007689.png

What causes this problem and how can I fix it, thanks.

Best regards.

Guofred

 

 

 

0 Kudos
Reply
1 Solution
5,115 Views
namnguyenviet
NXP Employee
NXP Employee

The problem is EB Tresos couldn't find the MCAL package. You need to install the MCAL package which correspond to the project you're using, by copy to the EB/tresos/plugins folder.

Best Regards,

Nam

View solution in original post

0 Kudos
Reply
2 Replies
5,116 Views
namnguyenviet
NXP Employee
NXP Employee

The problem is EB Tresos couldn't find the MCAL package. You need to install the MCAL package which correspond to the project you're using, by copy to the EB/tresos/plugins folder.

Best Regards,

Nam

0 Kudos
Reply
5,111 Views
Guofred
Contributor III

Hi @namnguyenviet ,

Ok, thanks for your help.

Best regards.

Guofred 

0 Kudos
Reply