i build a s32ds-arm2.2 project with example freertos_s32k146, i want:
make two task, one receive can data and del ,the other transmit responsed can data , and i use FLEXCAN_DRV_InstallEventCallback to send a queue, and receive task will receive it.
but i found that i cant make these tasks, even i use the same word with example, could anyone tell me why?
here is my code:
main.c:网络剪贴板 (netcut.cn)
rtos.c:网络剪贴板 (netcut.cn)
Solved! Go to Solution.
Hello @lc12138,
Maybe you can refer to this example:
Eventhough it is MCP5748G, it shows SDK FlexCAN in a FreeRTOS project.
BR, Daniel
Hello @lc12138,
Maybe you can refer to this example:
Eventhough it is MCP5748G, it shows SDK FlexCAN in a FreeRTOS project.
BR, Daniel