how to sppedup HSE initialization use IVT config

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

how to sppedup HSE initialization use IVT config

跳至解决方案
493 次查看
PINKMAN
Contributor III

hi expert:

i found that the HSE initialize time ia too long(50ms),i want to know how to   spped up HSE use  IVT config enable PLL.my chip is S32K312,Crystal oscillator iS 20MHZ, PLL PHI0 is 120MZ

PINKMAN_0-1751951742888.png

 

0 项奖励
回复
1 解答
418 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

It seems that you did not download the Example code corresponding to AN744511-Secure Boot Application note v0.1.1.0(1.1).pdf:

sw745310 SecureBootAppNoteDemo PDF Rev 1.0 Apr 4, 2022 28.61 MB

sw745310 SecureBootAppNoteDemo\SourceCode\src\main.c

/* enable utest fxosc usage and dcf clock option
* with pll enable in ivt.beq, secure boot verification can be accelerated */
EnableFXOSCUsage();

ChangeDcfClockOption();

The latest s32k3_hse_lib_rtd400hf01_20250627.7z also includes this function. Considering that you are a Chinese customer, it is recommended to contact FAE to obtain it.

 

在原帖中查看解决方案

4 回复数
472 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Have you referred to the methods described in chapter 9.3. Improve performance of Secure Boot Application note v0.1.1.0?

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
461 次查看
PINKMAN
Contributor III

hello:

i know the sequence is that config clock frequency and  HSE clock option in UTEST,AND then the BCW bit PLL_ENABLE AND BOOT SEQ will make sense.

in the startup_cm7.s ,I open the PLL_ENABLE AND BOOT SEQ as below

.long (CM7_0_ENABLE << CM7_0_ENABLE_SHIFT) | (CM7_1_ENABLE << CM7_1_ENABLE_SHIFT) | (CM7_2_ENABLE << CM7_2_ENABLE_SHIFT) | (CM7_3_ENABLE << CM7_3_ENABLE_SHIFT) | (PLL_ENABLE << PLL_ENABLE_SHIFT) | (BOOT_SEQ_ENABLE << BOOT_SEQ_ENABLE_SHIFT)

PINKMAN_0-1751963826089.png

but i don't know how to write UTEST?

 

 

0 项奖励
回复
419 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

It seems that you did not download the Example code corresponding to AN744511-Secure Boot Application note v0.1.1.0(1.1).pdf:

sw745310 SecureBootAppNoteDemo PDF Rev 1.0 Apr 4, 2022 28.61 MB

sw745310 SecureBootAppNoteDemo\SourceCode\src\main.c

/* enable utest fxosc usage and dcf clock option
* with pll enable in ivt.beq, secure boot verification can be accelerated */
EnableFXOSCUsage();

ChangeDcfClockOption();

The latest s32k3_hse_lib_rtd400hf01_20250627.7z also includes this function. Considering that you are a Chinese customer, it is recommended to contact FAE to obtain it.

 

477 次查看
PINKMAN
Contributor III
i change the IVT config as below,
(CM7_0_ENABLE << CM7_0_ENABLE_SHIFT) | (CM7_1_ENABLE << CM7_1_ENABLE_SHIFT) | (CM7_2_ENABLE << CM7_2_ENABLE_SHIFT) | (CM7_3_ENABLE << CM7_3_ENABLE_SHIFT) | (PLL_ENABLE << PLL_ENABLE_SHIFT)
but it didn't work
0 项奖励
回复