how to find the boot time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to find the boot time

2,214件の閲覧回数
ambarishhundeka
Contributor III

Hi NXP Team,

I am using the default configuration settings in our  project(S32K144 controller) , need to find the boot time(time between hardware reset to main).

how to find the boot time ?

is there any way to find the boot time in S32 Design studio IDE?

how much is the boot time for default configuration of the S32 Design project?

Regards,

Ambarish

ラベル(1)
1 返信

1,965件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

only boot time, which is defined, is time from power on reset to first executed instruction.

pastedImage_1.png

Time from first instruction to reach main function is application dependent, because there is startup code which can be different for every application.

It is not possible to find this time in S32 Design Studio, but you can simply measure this time.

Connect oscilloscope to reset line (first channel). Place the code which toggle some pin into your main function and connect the oscilloscope to this pin (second channel).

Now set trigger to reset line (change from logic 0 to logic 1) and measure the time to pin toggle.  

Regards,

Martin