how to disable s32K144 adc clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to disable s32K144 adc clock

1,609 Views
cuongtran
Contributor II

I want to set the S32K144 onto the very low power mode (VLPS) and disable the adc clocks as well.

0 Kudos
Reply
2 Replies

1,320 Views
aditya_barve
Contributor II

Can disabling the ADC modules by writing into ADCH register, be an option that can be considered in this case?

Thank you,
Aditya

0 Kudos
Reply

1,320 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,
Please have a look at Table 27-9, RM rev.7
You can disable both the Bus interface clock and the ADCLK in PCC module.

The bus interface clock is gated off by the transition to VLPS anyway.
And also, the FIRC, SOSC and SPLL clock sources must be disabled before the MCU enters VLPS (Section 27.4.4).

pastedImage_1.png


Anyway, the ADC module is idle when a conversion has completed and another conversion has not been initiated. When idle, the module is in its lowest power state.
If all triggers are disabled, the module stays idle (Section 42.5).

Regards,
Daniel

0 Kudos
Reply