how much minimum crrent does the input GPIO pin need about s32k?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how much minimum crrent does the input GPIO pin need about s32k?

1,034 Views
jinhui_wu
Contributor III

i am using s32k144,
i want to make a GPIO pin as input so that i can get external level on this pin.
i will connect a series resistor with the pin to limit the current.
i have a question,what's the value of series resistor ?
can i use a 1MΩ resistor?
I want to know that what's the minimum crrent does the input GPIO pin need?

Labels (1)
0 Kudos
1 Reply

782 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

If a pin is in Input mode, it does not need current.

This pin has high input impedance, the leakage current in typically only 0.005uA, max 0.5uA (Datasheet, Table 10).

Injection current is limited (max +-3mA) if the input voltage exceeds Vdd/Vss (Datasheet, Table 1). 

 

Regards,

Daniel

0 Kudos