eMIOS PWM output disable(OPWMB MODE)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eMIOS PWM output disable(OPWMB MODE)

ソリューションへジャンプ
1,539件の閲覧回数
FRIDAY618
Contributor II

hello experts:

when (OPWMB mode)PWM dutycylce is 100%, it can not be output disabled by ODIS register.

But if the dutycycle <100%,the (OPWMB mode) PWM can be disabled output by ODIS register.Such as the dutycle is 99% the PWM(OPWMB mode) can be disable by ODIS register.

And if the PWM mode is OPWFMB,it can be disbled by ODIS when it's dutycle is 100%.

why?And have any method to solve?

FRIDAY618_1-1729231871069.png

FRIDAY618_2-1729231892122.png

FRIDAY618_3-1729231907646.png

FRIDAY618_4-1729232169442.png

 

 

 

 

 

 

タグ(2)
0 件の賞賛
返信
1 解決策
1,477件の閲覧回数
FRIDAY618
Contributor II

FRIDAY618_0-1729501145812.png

FRIDAY618_1-1729501206920.png

FRIDAY618_2-1729501254757.png

 I used the demo but not solved problem?

I toggled gpio_34 pin and connect gpio_34 with PTB4(TRGMUX_in,1).when the pwm dutycle is 50%.it can be disabled by ODIS.

when the pwm dutycle is 100%.it still can not be disable.

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,478件の閲覧回数
FRIDAY618
Contributor II

FRIDAY618_0-1729501145812.png

FRIDAY618_1-1729501206920.png

FRIDAY618_2-1729501254757.png

 I used the demo but not solved problem?

I toggled gpio_34 pin and connect gpio_34 with PTB4(TRGMUX_in,1).when the pwm dutycle is 50%.it can be disabled by ODIS.

when the pwm dutycle is 100%.it still can not be disable.

 

 

 

0 件の賞賛
返信
1,473件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport
1,449件の閲覧回数
FRIDAY618
Contributor II

thanks,it works。i knew how to do。

タグ(1)
0 件の賞賛
返信
1,484件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@FRIDAY618

This is a test demo i made before and please have a try.

Senlent_0-1729494502461.png

 

0 件の賞賛
返信