Hello there,
We have several customers using our Microcontroller now. We have samples using s32k146 variant and some using s32k148. I was wondering if its possible to identify via register/function which MCU ID it is?
Because i have different linker scripts but somehow this was okay as i configured it for the smallest, but now i am using FlexRAM as EEPROM and DEPartitionCode is different. ( 0x08 / 0x04 )
Thanks.
Best regards,
Nader
已解决! 转到解答。
Hi naderkhamess,
Yes.
Please read the "11.3.1.8 System Device Identification Register (SDID)" of S32K1xx MCU Family - Reference Manual.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi naderkhamess,
Yes.
Please read the "11.3.1.8 System Device Identification Register (SDID)" of S32K1xx MCU Family - Reference Manual.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------