compiling error: S32K344 After D_CACHE_ENABLE is enabled

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

compiling error: S32K344 After D_CACHE_ENABLE is enabled

跳至解决方案
1,948 次查看
harryoceana
Contributor II

RTD 3.0.0 P07

S32DS 3.5

S32K344 After D_CACHE_ENABLE is enabled, the following error occurs when compiling. The cc.h file has many undefined macros

捕获.PNG

 

捕获.PNG

0 项奖励
回复
1 解答
1,890 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@harryoceana

D-cache is not supported in this routine, if you want to enable D-cache, this is suggestion from SW team.
You can add some following macros:

/* Data Cache masks */
#define DCACHE_CCR_EN_MASK             ((uint32)1U << 16U)
#define DCACHE_CSSELR_EN(x)            ((uint32)((x) & (~1U)))
#define DCACHE_DCCXSW_SET_MASK         ((uint32)0x3FE0U)
#define DCACHE_DCCXSW_SET_SHIFT        ((uint32)5U)
#define DCACHE_DCCXSW_WAY_MASK         ((uint32)0xC0000000U)
#define DCACHE_DCCXSW_WAY_SHIFT        ((uint32)30U)
/* Instruction Cache masks */
#define ICACHE_CCR_EN_MASK             ((uint32)1U << 17U)
#define ICACHE_CSSELR_EN(x)            ((uint32)((x) | 1U))
/* Cache set, way and line size */
#define CACHE_CCSIDR_SET_MASK          ((uint32)0xFFFE000U)
#define CACHE_CCSIDR_SET_SHIFT         ((uint32)13U)
#define CACHE_CCSIDR_SET_SIZE(x)       ((uint32)((((uint32)(x) & CACHE_CCSIDR_SET_MASK) >> CACHE_CCSIDR_SET_SHIFT) + 1U))
#define CACHE_CCSIDR_WAY_MASK          ((uint32)0x1FF8U)
#define CACHE_CCSIDR_WAY_SHIFT         ((uint32)3U)
#define CACHE_CCSIDR_WAY_SIZE(x)       ((uint32)((((uint32)(x) & CACHE_CCSIDR_WAY_MASK) >> CACHE_CCSIDR_WAY_SHIFT) + 1U))
#define CACHE_CCSIDR_LINE_SIZE_MASK    ((uint32)0x7U)
#define CACHE_CCSIDR_LINE_SHIFT        ((uint32)0U)
#define CACHE_CCSIDR_LINE_SIZE(x)      ((uint32)((((((uint32)(x) & CACHE_CCSIDR_LINE_SIZE_MASK) >> CACHE_CCSIDR_LINE_SHIFT) + 1U) * 4U) * 4U))

 

Test:

Senlent_0-1721297108982.png

 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,891 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@harryoceana

D-cache is not supported in this routine, if you want to enable D-cache, this is suggestion from SW team.
You can add some following macros:

/* Data Cache masks */
#define DCACHE_CCR_EN_MASK             ((uint32)1U << 16U)
#define DCACHE_CSSELR_EN(x)            ((uint32)((x) & (~1U)))
#define DCACHE_DCCXSW_SET_MASK         ((uint32)0x3FE0U)
#define DCACHE_DCCXSW_SET_SHIFT        ((uint32)5U)
#define DCACHE_DCCXSW_WAY_MASK         ((uint32)0xC0000000U)
#define DCACHE_DCCXSW_WAY_SHIFT        ((uint32)30U)
/* Instruction Cache masks */
#define ICACHE_CCR_EN_MASK             ((uint32)1U << 17U)
#define ICACHE_CSSELR_EN(x)            ((uint32)((x) | 1U))
/* Cache set, way and line size */
#define CACHE_CCSIDR_SET_MASK          ((uint32)0xFFFE000U)
#define CACHE_CCSIDR_SET_SHIFT         ((uint32)13U)
#define CACHE_CCSIDR_SET_SIZE(x)       ((uint32)((((uint32)(x) & CACHE_CCSIDR_SET_MASK) >> CACHE_CCSIDR_SET_SHIFT) + 1U))
#define CACHE_CCSIDR_WAY_MASK          ((uint32)0x1FF8U)
#define CACHE_CCSIDR_WAY_SHIFT         ((uint32)3U)
#define CACHE_CCSIDR_WAY_SIZE(x)       ((uint32)((((uint32)(x) & CACHE_CCSIDR_WAY_MASK) >> CACHE_CCSIDR_WAY_SHIFT) + 1U))
#define CACHE_CCSIDR_LINE_SIZE_MASK    ((uint32)0x7U)
#define CACHE_CCSIDR_LINE_SHIFT        ((uint32)0U)
#define CACHE_CCSIDR_LINE_SIZE(x)      ((uint32)((((((uint32)(x) & CACHE_CCSIDR_LINE_SIZE_MASK) >> CACHE_CCSIDR_LINE_SHIFT) + 1U) * 4U) * 4U))

 

Test:

Senlent_0-1721297108982.png

 

0 项奖励
回复
1,908 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@harryoceana

Could  you please describe clearly where the demo you are using comes from, what its name is, and what modifications you have made to it, so that we can reproduce the problem.

0 项奖励
回复
1,893 次查看
harryoceana
Contributor II

This is LWIP example, Only the D_CACHE_ENABLE definition was added .

1.PNG

 

2.PNG

 

0 项奖励
回复