compiling error: S32K344 After D_CACHE_ENABLE is enabled

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

compiling error: S32K344 After D_CACHE_ENABLE is enabled

Jump to solution
1,926 Views
harryoceana
Contributor II

RTD 3.0.0 P07

S32DS 3.5

S32K344 After D_CACHE_ENABLE is enabled, the following error occurs when compiling. The cc.h file has many undefined macros

捕获.PNG

 

捕获.PNG

0 Kudos
Reply
1 Solution
1,868 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@harryoceana

D-cache is not supported in this routine, if you want to enable D-cache, this is suggestion from SW team.
You can add some following macros:

/* Data Cache masks */
#define DCACHE_CCR_EN_MASK             ((uint32)1U << 16U)
#define DCACHE_CSSELR_EN(x)            ((uint32)((x) & (~1U)))
#define DCACHE_DCCXSW_SET_MASK         ((uint32)0x3FE0U)
#define DCACHE_DCCXSW_SET_SHIFT        ((uint32)5U)
#define DCACHE_DCCXSW_WAY_MASK         ((uint32)0xC0000000U)
#define DCACHE_DCCXSW_WAY_SHIFT        ((uint32)30U)
/* Instruction Cache masks */
#define ICACHE_CCR_EN_MASK             ((uint32)1U << 17U)
#define ICACHE_CSSELR_EN(x)            ((uint32)((x) | 1U))
/* Cache set, way and line size */
#define CACHE_CCSIDR_SET_MASK          ((uint32)0xFFFE000U)
#define CACHE_CCSIDR_SET_SHIFT         ((uint32)13U)
#define CACHE_CCSIDR_SET_SIZE(x)       ((uint32)((((uint32)(x) & CACHE_CCSIDR_SET_MASK) >> CACHE_CCSIDR_SET_SHIFT) + 1U))
#define CACHE_CCSIDR_WAY_MASK          ((uint32)0x1FF8U)
#define CACHE_CCSIDR_WAY_SHIFT         ((uint32)3U)
#define CACHE_CCSIDR_WAY_SIZE(x)       ((uint32)((((uint32)(x) & CACHE_CCSIDR_WAY_MASK) >> CACHE_CCSIDR_WAY_SHIFT) + 1U))
#define CACHE_CCSIDR_LINE_SIZE_MASK    ((uint32)0x7U)
#define CACHE_CCSIDR_LINE_SHIFT        ((uint32)0U)
#define CACHE_CCSIDR_LINE_SIZE(x)      ((uint32)((((((uint32)(x) & CACHE_CCSIDR_LINE_SIZE_MASK) >> CACHE_CCSIDR_LINE_SHIFT) + 1U) * 4U) * 4U))

 

Test:

Senlent_0-1721297108982.png

 

View solution in original post

0 Kudos
Reply
3 Replies
1,869 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@harryoceana

D-cache is not supported in this routine, if you want to enable D-cache, this is suggestion from SW team.
You can add some following macros:

/* Data Cache masks */
#define DCACHE_CCR_EN_MASK             ((uint32)1U << 16U)
#define DCACHE_CSSELR_EN(x)            ((uint32)((x) & (~1U)))
#define DCACHE_DCCXSW_SET_MASK         ((uint32)0x3FE0U)
#define DCACHE_DCCXSW_SET_SHIFT        ((uint32)5U)
#define DCACHE_DCCXSW_WAY_MASK         ((uint32)0xC0000000U)
#define DCACHE_DCCXSW_WAY_SHIFT        ((uint32)30U)
/* Instruction Cache masks */
#define ICACHE_CCR_EN_MASK             ((uint32)1U << 17U)
#define ICACHE_CSSELR_EN(x)            ((uint32)((x) | 1U))
/* Cache set, way and line size */
#define CACHE_CCSIDR_SET_MASK          ((uint32)0xFFFE000U)
#define CACHE_CCSIDR_SET_SHIFT         ((uint32)13U)
#define CACHE_CCSIDR_SET_SIZE(x)       ((uint32)((((uint32)(x) & CACHE_CCSIDR_SET_MASK) >> CACHE_CCSIDR_SET_SHIFT) + 1U))
#define CACHE_CCSIDR_WAY_MASK          ((uint32)0x1FF8U)
#define CACHE_CCSIDR_WAY_SHIFT         ((uint32)3U)
#define CACHE_CCSIDR_WAY_SIZE(x)       ((uint32)((((uint32)(x) & CACHE_CCSIDR_WAY_MASK) >> CACHE_CCSIDR_WAY_SHIFT) + 1U))
#define CACHE_CCSIDR_LINE_SIZE_MASK    ((uint32)0x7U)
#define CACHE_CCSIDR_LINE_SHIFT        ((uint32)0U)
#define CACHE_CCSIDR_LINE_SIZE(x)      ((uint32)((((((uint32)(x) & CACHE_CCSIDR_LINE_SIZE_MASK) >> CACHE_CCSIDR_LINE_SHIFT) + 1U) * 4U) * 4U))

 

Test:

Senlent_0-1721297108982.png

 

0 Kudos
Reply
1,886 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@harryoceana

Could  you please describe clearly where the demo you are using comes from, what its name is, and what modifications you have made to it, so that we can reproduce the problem.

0 Kudos
Reply
1,871 Views
harryoceana
Contributor II

This is LWIP example, Only the D_CACHE_ENABLE definition was added .

1.PNG

 

2.PNG

 

0 Kudos
Reply