code hangs on WDOG_EWM_IRQHandler() after Clear CCIF

cancel
Showing results for 
Search instead for 
Did you mean: 

code hangs on WDOG_EWM_IRQHandler() after Clear CCIF

666 Views
bhargavi_parali
Contributor I

Hello ,

I am trying to implement EEPROM functionality on s32k148 controller but code is getting hang after clearing CCIF bit and as well collision error detection bit (RDCOLERR) is getting set I checked in code watchdog interrupt bit  CS[INT] is disable and as well interrupt for CCIF bit (CCIE) is disable 

pastedImage_1.png

and if i restart the target without terminating or re - launching i don't face this issue 

Please find the attached code 

after further digging into this problem i  got to know that The Program Partition command must not be launched from flash memory,since flash memory resources are not accessible during Program Partition command execution.

Do we need to execute this function from RAM ? and How to do it ? 

i tried this doing by adding Macro START_FUNCTION_DEFINITION_RAMSECTION , but not working 

START_FUNCTION_DEFINITION_RAMSECTION
static uint8_t NVMT_CommandSequence(void)
{
uint8_t ret = TRUE;

/* Clear CCIF to launch command */
FTFC->FSTAT |= FTFC_FSTAT_CCIF_MASK;

/* Wait till CCIF bit is set*/
while(0U == (FTFC->FSTAT & FTFC_FSTAT_CCIF_MASK))
{

}

/*Check if any Error is occurred*/
if((FTFC->FSTAT & (FTFC_FSTAT_MGSTAT0_MASK | FTFC_FSTAT_FPVIOL_MASK | FTFC_FSTAT_ACCERR_MASK | FTFC_FSTAT_RDCOLERR_MASK )) != 0U)
{
ret = FALSE;
}

return ret;
}
END_FUNCTION_DEFINITION_RAMSECTION

in RM it was also mention that Changes related to execution of the Program Partition command take effect after the next
reset.

Do we need to do self reset after partitioning done ?       

Tags (1)
0 Kudos
1 Reply

585 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello bhargavi.paralikar@faurecia.com,

Please see the .map file in the Debug_Flash folder.

The command sequence function is in PFlash.

pastedImage_2.png

You can place the function to SRAM using this attribute:

__attribute__ ((section(".code_ram"))) // place the function below into .code_ram section
static uint8_t NVMT_CommandSequence(void);

Regards,

Daniel

0 Kudos