cannot access memory on adress 0x40024090

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

cannot access memory on adress 0x40024090

跳至解决方案
770 次查看
12914A
Contributor III

Hi,

I need to init FlexCAN0 and FlexCAN1. FlexCAN1 ist already working. 

At the init of FlexCAN0 it stops after the 4th loop of clearing the RAMn[] message buffers.

It shows the WDOG_EWM_IRQ_Handler(). At the EmbSys Register overview it shows at RAMn[5] the error message: cannot access memory on adress 0x40024090.

What can I do to solve this problem?

Best regards

Sandra

标记 (2)
0 项奖励
回复
1 解答
744 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if the module is clocked and enabled and you access valid address, which the MB area is, no fault is expected.
Hard to say, check above or share simplified project.

BR, Petr

在原帖中查看解决方案

0 项奖励
回复
1 回复
745 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if the module is clocked and enabled and you access valid address, which the MB area is, no fault is expected.
Hard to say, check above or share simplified project.

BR, Petr

0 项奖励
回复