XRDC in s32k344 running in lockstep mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

XRDC in s32k344 running in lockstep mode

Jump to solution
1,340 Views
FabioG
Contributor III

HI There

in XRDC module in a s32k344 running in lockstep , I read in manual that  master core could be CM7 or AHBP or AXI. So i am convinced that a s32k344 in lockstep mode is to referring to a AHBP core master access, is it true?

in RTD4.0.0 in   Rm RTD module ,the  core types are the following:

typedef enum
{
XRDC_CORE_M7_0 = 0x00U,
XRDC_CORE_HSE = 0x03U,
XRDC_CORE_M7_1 = 0x04U
} Xrdc_Ip_MasterCoreType;

It seams that lockstep configuration is not suited for these RTD ...?

What is the situation about XRDC in lockstep mode for s32k344 ?

best regards,

Fabio

 

0 Kudos
Reply
1 Solution
1,314 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @FabioG 

A small explanation of how Lockstep Core works is that two identical processors are initialized to the same state, and they receive the same inputs (code, bus operations, and asynchronous events), so during normal operation, the two processors operate in parallel, executing the same set of instructions simultaneously. The key feature of lockstep is that both cores execute the same instructions and compare their results at every step to ensure they match. If a discrepancy is detected, it indicates a potential error or fault in one of the cores, triggering a fault-handling mechanism.

Because of this behavior, in lockstep, there is only a reference to M7_0 and M7_1 would be N/A. 

 

B.R.

VaneB

View solution in original post

0 Kudos
Reply
2 Replies
1,315 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @FabioG 

A small explanation of how Lockstep Core works is that two identical processors are initialized to the same state, and they receive the same inputs (code, bus operations, and asynchronous events), so during normal operation, the two processors operate in parallel, executing the same set of instructions simultaneously. The key feature of lockstep is that both cores execute the same instructions and compare their results at every step to ensure they match. If a discrepancy is detected, it indicates a potential error or fault in one of the cores, triggering a fault-handling mechanism.

Because of this behavior, in lockstep, there is only a reference to M7_0 and M7_1 would be N/A. 

 

B.R.

VaneB

0 Kudos
Reply
1,250 Views
FabioG
Contributor III

Hi There,

Referring Figure8 Block Diagram page 24 Reference manual:

FabioG_0-1712833197713.png

 

It seems that CM7_1 accesses to bus via MDAC4, when XRDC is enabled. So in Lockstep mode i have to manage only MDAC0 (CM7_0)?

Regards

Fabio

0 Kudos
Reply