XRDC Memory regions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
398件の閲覧回数
FabioG
Contributor III

 

HI there,

I don't understand the cross reference between MRC Slave protected PFLASH_0, PFLASH_1,...PFLASH_WR, ...,PRAM0,PRAM1 (see below)

FabioG_2-1712823602437.png

and the s32k3xx_Memory Maps where FLASH splitted in program flash data flash  and ram is splitted in SRAM0,1,2 (see below). I need to know that in order to configure xrdc configurations

Can you help me ?

 

FabioG_1-1712823563810.png

 

0 件の賞賛
返信
1 解決策
357件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @FabioG,

You can see the ports in the block diagram.

Figure 8. Block diagram – S32K324, S32K344 and S32K314

danielmartynek_0-1712913592825.png

 

The PFLASH_WR port is for writting/programming the flash (not depicted), while other ports are just for reading.

danielmartynek_0-1713253499220.png

Refer to RM sections:

22.1.1 Flash memory architecture

23.1 Chip-specific PRAMC information

 

Regards,

Daniel

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
358件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @FabioG,

You can see the ports in the block diagram.

Figure 8. Block diagram – S32K324, S32K344 and S32K314

danielmartynek_0-1712913592825.png

 

The PFLASH_WR port is for writting/programming the flash (not depicted), while other ports are just for reading.

danielmartynek_0-1713253499220.png

Refer to RM sections:

22.1.1 Flash memory architecture

23.1 Chip-specific PRAMC information

 

Regards,

Daniel

 

0 件の賞賛
返信