Will CANFD message ignored by CAN1 and CAN2 on S32K144?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Will CANFD message ignored by CAN1 and CAN2 on S32K144?

跳至解决方案
681 次查看
liguangyu02
Contributor II

Dear community,

In my porject with S32K144, the CAN0 already used for a CAN-FD bus. However there is needed to connected CAN1 or CAN2 to a bus with both CAN-FD message and standard can message.

So my question is: for CAN-FD message, will CAN1/CAN2 just ignore it or treat it as error frame?

Thanks!

Guangyu

0 项奖励
1 解答
665 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@liguangyu02

      CAN1 and CAN2 channels do not support CAN FD, if a CAN FD frame is received, it should be recognized as an error frame.

在原帖中查看解决方案

2 回复数
663 次查看
liguangyu02
Contributor II

Thank you Senlet for the quick reply!

BRs

Guangyu

0 项奖励
666 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@liguangyu02

      CAN1 and CAN2 channels do not support CAN FD, if a CAN FD frame is received, it should be recognized as an error frame.