Will CANFD message ignored by CAN1 and CAN2 on S32K144?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Will CANFD message ignored by CAN1 and CAN2 on S32K144?

Jump to solution
1,518 Views
liguangyu02
Contributor II

Dear community,

In my porject with S32K144, the CAN0 already used for a CAN-FD bus. However there is needed to connected CAN1 or CAN2 to a bus with both CAN-FD message and standard can message.

So my question is: for CAN-FD message, will CAN1/CAN2 just ignore it or treat it as error frame?

Thanks!

Guangyu

0 Kudos
Reply
1 Solution
1,502 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@liguangyu02

      CAN1 and CAN2 channels do not support CAN FD, if a CAN FD frame is received, it should be recognized as an error frame.

View solution in original post

2 Replies
1,500 Views
liguangyu02
Contributor II

Thank you Senlet for the quick reply!

BRs

Guangyu

0 Kudos
Reply
1,503 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@liguangyu02

      CAN1 and CAN2 channels do not support CAN FD, if a CAN FD frame is received, it should be recognized as an error frame.