Why must open the ‘EcuM WakeUP source’ parameter when configuration the Lin moudle in MCAL EB tresos

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why must open the ‘EcuM WakeUP source’ parameter when configuration the Lin moudle in MCAL EB tresos

1,758件の閲覧回数
ananan
Contributor III

As shown below, when I do not configure the EcuM WakeUP Source, an error is reported at compile time in the red box below

ananan_0-1636005421975.png

But when I add the EcuM module (add the WakeUP source) and it turns on the EcuM WakeUP Source, the error disappears

ananan_1-1636005734480.png

I don't want to use Ecum module, and I don't want to turn on LIN wake up function, how should I configure, I don't know what to do

0 件の賞賛
返信
1 返信

1,745件の閲覧回数
hungnguyenphi
NXP Employee
NXP Employee

Hello @ananan ,

 

This is a limitation in the MCAL_4.3_RTM_1.0.1. Could you please try the newest version MCAL_4.3_RTM_1.0.2.

 

Best regards,

Hung.

0 件の賞賛
返信