Hello,
When I try to use LPIT0 module as a periodic timer, it doesn't work at all. And then, I find that all the registers except VERID are 0xFFFFFFFF. Why?
I would really appreciate it if anyone could give me a answer.
Best regards,
Ashlie
Sorry, I just find that it's the compiler display issue. The lpit0 configuration is ok. It never comes into the interrupt I want but runs into a defaultISR when I configure a interrupt enable in EBTresos as the picutre:
Maybe it's because I didn't add the interrupt handler into vector table.But what should I do for the next step?
Sorry, I am not familiar with EB tools,you can create a new topic on this forum.
next time,please remember to fill in the complete part number and add some key words in your topic,such as MCAL,EB ,etc, so that your issues will be resloved much faster.