Where does the program start running after S32K344 wakes up from standby?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Where does the program start running after S32K344 wakes up from standby?

跳至解决方案
1,234 次查看
SCoder41
Contributor III

Where does the program start running after S32K344 wakes up from standby?

0 项奖励
回复
1 解答
1,216 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

System reset -> HSE_B sBAF -> startup code(reset_handler) -> application


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
8 回复数
1,217 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

System reset -> HSE_B sBAF -> startup code(reset_handler) -> application


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
1,200 次查看
SCoder41
Contributor III
Our S32K344 manages the power management chips that supply power to other modules, and requires S32K344 to enable these power management chips. If I wake up S32K344 from standby mode, it will perform a system reset from the reset handler to run the program, and other modules on our board will lose power. How can I solve this problem?
0 项奖励
回复
1,193 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Please tell me the part number of power management chip. If you only need to maintain the S32K3 pin voltage, please read 7. Pad keeping in Standby mode of S32K3xx Low Power Management.pdf

0 项奖励
回复
1,181 次查看
SCoder41
Contributor III
TPS62135、TPS54J061RPGR and BQ25171Q1。Can I maintain the high output level of S32K344 gpio pin during the system reset period when S32K344 wakes up?
0 项奖励
回复
1,175 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Yes.

Have a look at the Figure 8. Pad keeping flow of S32K3xx Low Power Management.pdf. All pins retain its last state from run mode during standby.
No matter pad keeping is enabled or not before going to standby mode, the GPIO will always retain the status set before going to standby mode. The function of pad keeping is mainly keep the GPIO mode between MCU reset to pad keeping disable(write DCM_GPR->DCMRWF1[STANDBY_IO_CONFIG] = 1).

0 项奖励
回复
1,172 次查看
SCoder41
Contributor III
So when my MCU wakes up from standby mode to RUN mode, can I keep the GPIO output high all the time?
0 项奖励
回复
1,165 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Yes. Set the GPIO high and then write 1 to DCMRWF1[STANDBY_IO_CONFIG]:

Set GPIO high and then set STANDBY_IO_CONFIG.png

It is recommended to use an oscilloscope to confirm the pin status.

0 项奖励
回复
1,159 次查看
SCoder41
Contributor III
thanks
0 项奖励
回复