Hi guys, I am implementing the low power mode function.
The aim is to enter VLPS mode, and wake up the MCU from VLPS by LPTMR every 80ms.
After wake up, enable LPIT with period 600us to trigger AD function.
Now, the issue is the period of LPIT is not correct.
The designed period is 600us, but the measured period is 4ms or so.
The incorrect period is just happened at the first cycle after waked up from VLPS. The afterward period is quit correct.
Some other information:
LPTMR: clock source is SIRC.
LPIT: clock source is SIRC.
Chip: S32K148
Could anyone help me ? Thanks in advance.