When i use multlink unversal, the i2c can't work.
But when I use jlink or run it directly in flash, i2c can work properly.
Can u help me?
 VaneB
		
			VaneB
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi @zyc0211
As you can run the project using J-LINK the problem looks not to be related to the code. The debug configurations or the linker files could be the cause of it. Could you please test if, with an example code, you present the same behavior?
Also, verify if the PEmicro multilink universal is not damaged and is correctly connected.
B.R.
VaneB
 VaneB
		
			VaneB
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi @zyc0211
Are there any hardware differences between the EVB and your prototype? Please check all connections and if necessary reconnect them.
Do you have more prototypes? If yes could you please test if the same behavior is also present?
I don't have more prototypes.
Can you tell me what hardware differences might have caused this?
 VaneB
		
			VaneB