Hi @simon98
In the transmission I made, I set SpiDataWidth to 8 bits, which matches the size of each data element I am transmitting. I also defined SpiEbMaxLength as 100, which represents the maximum number of data elements that can be transmitted in a single operation.
Although I transmitted an array of 10 data elements, each 8 bits wide, since SpiEbMaxLength was set to 100, I have the capacity to transmit up to that limit. In this case, since I only sent 10 data elements, we did not reach the maximum allowed, but if necessary, I could transmit up to 100 data elements in a single operation without any issues.
Hi @simon98
The SpiDataWidth parameter represents the frame size in terms of the number of bits. For MCAL, the maximum frame size is 64 bits, as it is designed to be compliant with AUTOSAR 4.7, according to the "Specification of SPI Handler/Driver" documentation provided by AUTOSAR.
The SpiEbMaxLength refers to the maximum number of data elements that can be stored in the external buffer.
BR, VaneB
Hi @simon98
In the transmission I made, I set SpiDataWidth to 8 bits, which matches the size of each data element I am transmitting. I also defined SpiEbMaxLength as 100, which represents the maximum number of data elements that can be transmitted in a single operation.
Although I transmitted an array of 10 data elements, each 8 bits wide, since SpiEbMaxLength was set to 100, I have the capacity to transmit up to that limit. In this case, since I only sent 10 data elements, we did not reach the maximum allowed, but if necessary, I could transmit up to 100 data elements in a single operation without any issues.