( please refer to the following diagram)
Hi jingfang,
This is a voltage range of a single domain.
This is an internal signal, not necessarily needed for the customer to develop their applications.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Yes, but will it be convenient? Because the terminal wants to know.
The SRAM data are retained across any system reset except for Power-on reset.
But in order to by sure it is not overwritten, we can clear the SRAMU_RETEN & SRAML_RETEN bits.