What is the time for the S32K1's power supply to rise to the RESET pin?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is the time for the S32K1's power supply to rise to the RESET pin?

3,091 次查看
jingfang
Contributor IV

What is the time for the S32K1's power supply to rise to the RESET pin?

0 项奖励
回复
4 回复数

3,069 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @jingfang,

It depends on the power supply ramp rate:

danielmartynek_3-1690874790095.png

Once VDDX reaches 2.7V, which is the Low Voltage Reset Deassert threashold, the MCU leaves the system reset.

danielmartynek_2-1690874763315.png

In the datasheet, you can find these specifications:

 

danielmartynek_0-1690874384671.png

 

Regards,

Daniel

0 项奖励
回复

2,804 次查看
Nibesh
Contributor III

Hello @danielmartynek 
Thank you very much for your clarification. I have understood it.
But if can you tell me roughly, how much time it will take to jump to Application, when we normally Reset the MCU.
Actually I am achieving 4.22ms, for your kind reference I have attached Logic Analyzer image.
I hope you will correlate my doubts.

One more Doubts @danielmartynek  

Will you clarify my one Doubts, on the Datasheet the Flash Timing Specification for (Program Section
execution time) (1KB flash)  is 5ms.
So when the Micro-controller is Powered, does it is taking 5ms to jump into the Application Program?
For you kind reference I took snap from the datasheet. I hope you will check Flash Timing Specifications Image for it.

I hope to hear from you Soon

BR 
Nibesh

0 项奖励
回复

2,795 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Nibesh,

Can you put it into a new thread?

This is not related to the subject of this thread.

 

Regards,

Daniel

0 项奖励
回复

2,792 次查看
Nibesh
Contributor III
Yeah Sure will keep on new thread Daniel.

Thank you.
0 项奖励
回复