Hi@youngyanliang
FTM can full-function run on VLPR mode only when source by SIRC, so the FTM source clock frequency is 8MHz default,and the max clock source prescaler is 128,
So the FTM max overflow time is :(63335-1) / (8000000Hz / 128) =1.048544S,I guess.
in this case,the LED frequency is so slow, is it necessary to use the FTM module?
BR!
Jim,