What is the difference between ADCP,ADCSA and ADCE on S32K3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the difference between ADCP,ADCSA and ADCE on S32K3

Jump to solution
1,397 Views
Guofred
Contributor III

Dear Sir,

What is the difference between ADCP,ADCSA and ADCE on S32K3

ADCP: Precision mode, the covert data width is around 15

ADCS: Standard mode,  it is normal mode, 12bit ADC

ADCE: External mode , one multiplexer has 8 channels,  4 multiplexer are around 32 channels.

we can set the MCR registor to Enable the different ADC conversion mode, my understanding is right or

not, would you like kindly help to share your comments, thanks.

Guofred_0-1659074177690.png

Guofred

 

 

0 Kudos
1 Solution
1,382 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

From functional point of view ADC conversions are the same with configurable resolution:

davidtosenovjan_1-1659430141256.png

 

The difference see in datasheet specification:

davidtosenovjan_0-1659430042301.png

 

View solution in original post

0 Kudos
5 Replies
1,389 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I don't understand your description too much.

There are three typed of ADC channels on the device. Standard and Precision differs in offered precision, external channels offering adding of external multiplexer to increase number of inputs.

0 Kudos
1,028 Views
Niuyanlin
Contributor I
Hello! How to use S32K3 ADC External channels? I'm not sure how to use it
0 Kudos
1,386 Views
Guofred
Contributor III

Hi @davidtosenovjan ,

Yes, thanks for your kindly help.

would you like kindly help to share the differ of the offered precision between standard and precision.

such as standard type ADC channel has 12 bit resolution,  precision type ADC channel has 15 bit

resolution, my understanding is right or not, kindly help to share your comments, thanks. 

Best regards.

Guofred

0 Kudos
1,383 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

From functional point of view ADC conversions are the same with configurable resolution:

davidtosenovjan_1-1659430141256.png

 

The difference see in datasheet specification:

davidtosenovjan_0-1659430042301.png

 

0 Kudos
1,379 Views
Guofred
Contributor III

Hi @davidtosenovjan ,

yes, thanks for your kindly help.

 

Best regards.

Guofred

0 Kudos