As the question head saying, I don't know what is the CSEc key, BOOT_MAC's debug protect attribute use for. I have tried to set this attribute, and found secure boot will also be succeed with debug attatched, would you give me some explains? thank you very much!
BR,
yaojianhang.
解決済! 解決策の投稿を見る。
OK, in case of BOOT_MAC, I can see that it really doesn't work as expected. Thanks for pointing this out, I will report it. The workaround is simple here - set this attribute for BOOT_MAC_KEY instead of BOOT_MAC. It is sufficient if at least one of them is set. The effect will be the same.
Regards,
Lukas
Hi @yaojianhang
not sure how you tested this but it works as expected on my side...
This is a state when I turn on the board and connect a debugger without reset (hot attach):
If debugger is connected and if I reset the board via debugger:
So, I can see no problem here.
How did you set the attribute? I used AN5401 for my test and I used:
calculate_M1_to_M5(M1, M2, M3, M4, M5, MASTER_ECU_KEY_VALUE, BOOT_MAC_KEY_VALUE, MASTER_ECU_KEY, BOOT_MAC_KEY, 1, 0b001000);
Regards,
Lukas
OK, in case of BOOT_MAC, I can see that it really doesn't work as expected. Thanks for pointing this out, I will report it. The workaround is simple here - set this attribute for BOOT_MAC_KEY instead of BOOT_MAC. It is sufficient if at least one of them is set. The effect will be the same.
Regards,
Lukas