Hello NXP team.
I am using the S32K144 microcontroller.
I want to wake up the MCU from VPLS using GPIO.
Do you have a ready example using RTD?
S32K144EVB
解決済! 解決策の投稿を見る。
Hi @adem_marangoz,
In your other community thread, you mentioned using the legacy SDK v3.0.0:
https://community.nxp.com/t5/S32K/Wake-the-MCU-from-VLPR-using-a-GPIO-pin/m-p/2198256#M54116
This SDK includes a default example that demonstrates low-power modes, including VLPS.
Regards,
Daniel
元の投稿で解決策を見る
Hello @adem_marangoz,
Let me check.
Do you need MCAL or IP example?
What do you mean by the Freescale Semiconductor libraries?
The S32K1xx RTD has
Does it mean you need an example with the Ip drivers?