Hello Sir ,
I am facing a issue with my design
problem statement:-I am converting a voltage from 12V to 4.7V with the help of zener diode
combination ,and the voltage i am reading directly to S32KMCU
But once i am conncting the trace to the ADC pin for measurement of voltage 4.7V i am not getting the voltage excetly 4.7V i am getting around 1.8V
and Once i disconnect the trcae to the MCU i am getting expected voltage 4.7V
can you please suggest possible solution
Hello,
Can you share the exact MCU type and the pin, where is 4.7V connected?
If the supply voltage of the connected pin is lower than 4.7V, then the voltage will be limited to the supply voltage. Or the pin is not in highZ state, it might be in a logic low level. You can check that as well.
Best regards,
Pavel
MCU is S32K341,PIN is PTA15/ADC1
the ADC VREF supply voltage is 5V.
But I have not powerd the MCU .I have just connected the trace to ADC pin for measurement .
Hi,
in that case, the MCU is powered from the pin (via diode between pin and VDDx) and the voltage drop is a logical consequence. If I were you I would try to avoid this behavior.
Best regards,
Pavel
Okey noted
So how will you connect the 4.7V to MCU ADC pin in order to not get dip in voltage
1:- using buffer circuit
2:-using a voltage dividers
Any suggestions from your side
Regards
Praveen