VREFH for S32K324

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VREFH for S32K324

Jump to solution
2,106 Views
hemanths
Contributor III

Hi NXP Team,

I am using the S32K324 microcontroller operating at 3.3V for my circuit. The VREFH pin in the microcontroller is connected with 3.3V (VDD_HV_A / VDD_HV_B) itself. In the datasheet, I saw a note regarding the VREFH voltage levels.

hemanths_0-1688361073670.png

But in the hardware design guidelines document this comment is not mentioned.

hemanths_1-1688361175410.png

Can somebody please explain the significance of the note mentioned in the datasheet.

 

Thanks & Regards

Hemanth 

 

0 Kudos
Reply
1 Solution
2,087 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Hemanth,

The VREFH reference does not have to be connected to VDD_HV_A / VDD_HV_B.

But the reference is clamped to VDD_HV_A, therefore, the voltage must not exceed VDD_HV_A + 0.1V, and the 0.1V is for RF signal only.

In the HWDG rev.C, you can find the specification too:

danielmartynek_0-1688380987606.png

 

Regards,

Daniel

 

 

View solution in original post

0 Kudos
Reply
3 Replies
2,088 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Hemanth,

The VREFH reference does not have to be connected to VDD_HV_A / VDD_HV_B.

But the reference is clamped to VDD_HV_A, therefore, the voltage must not exceed VDD_HV_A + 0.1V, and the 0.1V is for RF signal only.

In the HWDG rev.C, you can find the specification too:

danielmartynek_0-1688380987606.png

 

Regards,

Daniel

 

 

0 Kudos
Reply
2,077 Views
hemanths
Contributor III

Hi Daniel,

Thanks for the response.

What happens if the input voltage of an ADC is greater than the VREFH of the ADC? Whether the microcontroller's ADC have any overvoltage protection or saturation mechanisms?

0 Kudos
Reply
2,071 Views
danielmartynek
NXP TechSupport
NXP TechSupport

The ADC result would be saturated.

The injection current must be limited to 3mA per a pin.

danielmartynek_0-1688384914242.png

danielmartynek_1-1688385147391.png

 

BR, Daniel

 

0 Kudos
Reply