Using one TRGMUX source for multiple target module?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using one TRGMUX source for multiple target module?

Jump to solution
1,338 Views
JeorgeB
Contributor III

Is that possible to use one TRGMUX source for multiple target modules in S32K14x? 

e.g., FTM0_INIT_TRIG to (DMA_CH0, ADC0_ADHWT, LPUART0_TRG and LPSPI0_TRG)

 

 

Thanks.

 

0 Kudos
Reply
1 Solution
1,313 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, I believe it should works. Configuration is not mutually exclusive, so could be able to assign TRGMUX input to multiple outputs.

View solution in original post

0 Kudos
Reply
1 Reply
1,314 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, I believe it should works. Configuration is not mutually exclusive, so could be able to assign TRGMUX input to multiple outputs.

0 Kudos
Reply