Using SENT as Triggered SENT using Flex IO peripheral

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using SENT as Triggered SENT using Flex IO peripheral

859 次查看
AVargh23
Contributor III

Can a FlexIO pin be used as an output to send trigger and then receive SENT frames for S32K344? The example project has it set up for FlexIo Sent Receiver alone. Is it possible to make use of the same to act as an output to send trigger pulses to SENT device  and then change it to input to receive the SENT frames? 

标记 (3)
0 项奖励
回复
1 回复

834 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, it is apparently not possible to do it with FlexIO. Pay attention to following thread:
https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-FlexIO-configuration-to-SENT-SAE-J2...

 

0 项奖励
回复