Using EB tresos to add some modules always fails to add

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using EB tresos to add some modules always fails to add

3,916件の閲覧回数
Brady_Li
Contributor I

Using EB tresos to add some modules always fails to add。

I can add baseNXP, platform, resource, safetyBase, but I can't add other modules. The error is as follows:
Cannot add node of type "BooleanSchemaNode(NAME=POST_BUILD_VARIANT_USED, TYPE=BOOLEAN, VALUE=)" to "MODULE-DEF"

Error in file "crypto:///C:/NXP/EB/../SW32K3_S32M27x_RTD_R21-11_4.0.0_HF01/eclipse/plugins/Adc_TS_T40D34M40I0R0/config/Adc.xdm", line "6861": (1005) Cannot add node of type "BooleanSchemaNode(NAME=POST_BUILD_VARIANT_USED, TYPE=BOOLEAN, VALUE=)" to "MODULE-DEF"

Can you tell me the reason and how to solve it?

0 件の賞賛
返信
4 返答(返信)

3,354件の閲覧回数
kenneth_atV
Contributor I

 am using tresos Studio, 24.0.1 and the same problem with 29.0.0

I installed RTD:

S32K1_S32M24X Real Time Drivers AUTOSAR R21-11 Version 2.0.0 P04


and I am getting the same error. I tried looking for RTD 4.0.0 P24, but I cannot find anything that matches this.
The error shows in the XDM files, so I am stuck and not able to add any modules. Any ideas?


0 件の賞賛
返信

3,893件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Brady_Li,

Could you share your EB Tresos version? Also, you can try removing and re-adding the ADC plugin into the "plugins" folder.

Could you also test if by importing an example, or a blank project, the same error occurs?

Best regards,
Julián

0 件の賞賛
返信

3,848件の閲覧回数
Brady_Li
Contributor I

Version information, error information such as pictures,

The version information reminded me that I originally wanted to install 29.0, but some errors may have occurred. I just noticed that the current version is 24.0

0 件の賞賛
返信

3,830件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Brady_Li,

Could you try installing a different release for the 4.0.0 package? Since the Hot Fix Releases are not fully qualified and are not intended for production, they must be replaced by the next qualified standard release.

Any of the full releases should work (RTD 4.0.0 P24 is the latest as of now).

Best regards,
Julián

0 件の賞賛
返信